This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: How to add more RAM

Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE, TMDSCNCD28379D, CONTROLSUITE,

Tool/software:

Hi, I am exploring an option of adding more RAM to the F28379D chip.

At present, the chip has 1024 kByte Flash and 204 kByte RAM. If my code increases or I want to run it at a faster sample time (faster execution period), I would need more RAM memory. Is it possible to add more RAM (e.g., IS61WV5128BLL-10TL), and how do I connect it to F28379D?

Size up DSPs: F28388D with 1536 kByte Flash and 338 kByte RAM and F29H850 with 4864 kByte Flash and 452 kByte RAM are as a last resort if RAM upgrade does not work.

F28379D pin layout (from https://www.ti.com/lit/gpn/tms320f28379d, Fig. 5-5, Page 13

RAM pin layout (from http://www.issi.com/ww/pdf/61-64wv5128axx-bxx.pdf, Page 2)

If this is successful, are there any settings in the application (e.g., MATLAB Simulink), or will the F28379D automatically recognise and use additional RAM?

Regards, MB