Part Number: TMS320F280037C
Tool/software:
Hi Champ,
I am asking for my customer.
(1). They do ADC conversion, would the converted digital result still be linear when sampling voltage is less than 0.1V ?
Since they sample an analog input voltage which is less than 30mV, the converted digital result doesn't seem to get the value from analog to 12-bit Digital Formula.
(2). Is there a characteristic representing ADC sampling linearity ?
(3). What's the min. effective sampling voltage for the device ?
Thanks for the input.
Regards,
Johnny