This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P650DH: complier fail

Part Number: TMS320F28P650DH
Other Parts Discussed in Thread: C2000WARE

Tool/software:

when i compile project of c2000 in CCS20,  CCS shows " Product C2000WARE v5.2.0.00 is not currently installed and no compatible version is available. Please install this product or a compatible version

  • Hi Claud,

    1. First Solution - Clean Installation: (0)

    • Uninstall any existing C2000WARE installations
    • Uninstall CCS
    • Reboot your computer
    • Install the latest version of CCS (currently CCS 12.7)
    • Download and install C2000WARE v5.2.0.00 from ti.com
    2. If the error persists, check the project properties: (2)
    • Right-click on your project and go to Properties
    • Under General -> Products, verify that C2000WARE 5.2.0.00 is listed and selected
    3. Workspace Solution: If the above steps don't work:
    • Create a new workspace
    • Remove any old C2000WARE versions that could conflict
    • Re-download C2000WARE 5.2.0.00 from ti.com
    • Import your project into the new workspace
    4. Path Verification: 
    • Double-click on the C2000WARE software package in CCS
    • Go to preferences
    • Verify it's pointing to the correct installation directory
    • Make sure there are no conflicts with older versions
    References:
    BR,
    Ryan Ma