This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P650SK: CCS20.2.0 QUESTION. How to display Assembler labels in the Editor. PLEASE HELP, URGENT.

Part Number: TMS320F28P650SK


Tool/software:

Hi Guys. Is there a way of displaying my assembler LABELS in a window in CCS 20.2.0.? 

In CCS 12.8.1 to see my assembly labels in my asm.s program I click on the arrow next to my asm.s file in PROJECT EXPLORER and the arrow spins to the down direction and then my labels are listed. ( Oh I'm using a iMac OS X 10.15.7 ) .

Then I just double click on a label and the editor jumps to the label in my ASM code. 

I'm getting tired of scrolling up and then back down again to find my subroutines. PLEASE don't tell me to go into the Disassembly window and look at my labels there, that only works when I debug my asm program.

I need to view my labels in the editor while I'm writing my asm code.

Also because my program size is 601k (at present)  CCS12.8.1 will not write the full flash as there is a bug. I was told to use CCS 20.2.0 as this bug has been fixed which it has and it works perfectly.

Please let me know how to do this as this is driving me absolutely crazy.

Thanks and hope to hear from you soon.

Peter Slight smile