Part Number: TMS320F28P650SK
Other Parts Discussed in Thread: LAUNCHXL-F28P65X
Tool/software:
Hi guys, I'm have a serious problem with port toggle speed. I'm using CCS 20.2.0 with iMac OS 10.15.7.
I have written a small assembler program toggling the full 32bit PORT A pins. I've set the PLL to 55Mhz. The PLL clock source is IntOsc2. I've enabled the XCLKOUT pin so I can read the CPU speed with my scope.
Here's the problem.
When I debug my assembler program in CCS 20.2.0 the program runs. The CPU speed reads at 55.5Mhz and PORTA toggle speed reads at 2.2Mhz. Ok, I'm happy with that.
Now when I power off my stand alone board and then power it back on to see if codestart is actually working this is the read outs I get.
CPU speed is 55.5Mhz which is correct and PORTA toggle speed is only 31.4Khz. What happened to PORTA toggle speed?
It's exactly the same code when I run it in CCS20.2.0.
What I need is when I debug and then power off then power on I need it to be the same speed every time.
Please let me know if I need to setup some other registers to fix the PORTA toggling speed problem.
Thanks guys, hope to hear from you soon.
Pete :)