Part Number: TMS320F280039
Other Parts Discussed in Thread: C2000WARE
Tool/software:
I've been trying to migrate to CCS v20.0.2 and use the C2000 IDEA extension. I've run into issues though with setting up the C2000 IDEA extension, as if the extension is unresponsive. I'm not sure if this is an application configuration issue, project settings issue or possibly an extension issue.
So far I have been able to create a workspace, add existing projects, create projects and successfully compile these projects (right now I have 3 projects within the workspace). When opening the C200 IDEA extension I navigate to "C2000 IDEA - Features" -> "Project detection" and select "Get Projects". The folder icon on the right responds to a click though I see no notification boxes appear or logs indicating an action is performed. Further more none of the 3 projects get detected and the "C2000 IDEA - Projects" section remains empty. The behaviour is the same when using the command palette (CTRL + SHIFT + P) and running "C2000: Get Projects".
I was hoping to get help in troubleshooting this to see if there's something I'm missing or an issue in how I currently have everything setup. I followed this guide for installation. https://www.ti.com/lit/an/spradl6a/spradl6a.pdf?ts=1753328974788
Cheers,
Matt