Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Greetings,
We are migrating to Windows 11, and I have been able to rebuild my C:\ti folder to the point where most of the projects build. The exception is the CLB projects. The output says that it cannot see "c2000ware_software_package v2.0.0.02". But I can see it in the C:\ti folder as shown below (the first item was an error, and the rest are warnings). It was installed using the installer. What else do I need to do to have the tools see it?
Description Resource Path Location Type
Product c2000ware_software_package v2.0.0.02 is not currently installed and no compatible version is available. Please install this product or a compatible version. <ProjectName> <ProjectName> Problem
Invalid project path: Include path not found (\device_support\f2837xd\common\include). <ProjectName> pathentry Path Entry Problem
Invalid project path: Include path not found (\driverlib\f2837xd\driverlib). <ProjectName> pathentry Path Entry Problem
Invalid project path: Include path not found (\utilities\clb_tool\clb_syscfg\systemc\include). <ProjectName> pathentry Path Entry Problem

Thank you,
Ed