Part Number: TMS320F28388D
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
hello,
I would like to use the SCI UART TX with GPIO 29 as the transmit port but I want to do it using the DMA channel.
There is no example for that in the C2000 examples folder (or at least I could not find such example)
I only found the "sci_ex1_loopback" example and I was able to change the GPIO ports there from 135 to 29 using the syscfg file.
and this worked fine.
Is it possible to make a change to this project and make it use the DMA for the TX?
Thanks.