This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28379D: LED blinking takes longer than 1 sec

Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: SYSCONFIG

Tool/software:

HI 

I am trying to use the timer with ISR to turn on and off the LED on the board after each second but it takes longer than 1 second to turn the led on and off, wondering if the clock frequency is 200 MHZ or by default it is less than that ? 

Kind Regards

  • Hi Sana,

    Can you share more details about your CPU timer configurations - which period and prescaler values are you using? Are you using Sysconfig for your configurations? The default SYSCLK frequency will likely be 200MHz for this device, yes. If using the LaunchPAD, make sure to add the below as a predefined symbol in your project so that the correct device initializations are executed.

    _LAUNCHXL_F28379D

    Best Regards,

    Delaney

  • HI Delaney 

    The _LAUNCHXL_F28379D worked, thank you very much for your help, appreciate it

    Kind Regards

    Sana