Part Number: TMS320F28377D
Tool/software:
Hi TI Team,
I have a question in regard to the Sample capacity of the four ADCs used in the TMS320F28377DPTPQ.
In the datasheet is only one typical value for the Sampling capacitor of 14,5pF.

I have a question: What are roughly the limits of this value max and min and is there a difference between all ADCs (A-D) in the controller?
BR FM
By the way: In the documentation of the use of the ADC is always Ch 12,5pF I think 14,5pF from the data sheet is right. (ADC Input Circuit Evaluation for C2000 MCUs (using TINA-TI simulation tool) (Rev. A); TMS320F2837xD Dual-Core Microcontrollers Technical Reference Manual (Rev. K))