Part Number: TMS320F28388D
Other Parts Discussed in Thread: UNIFLASH, C2000WARE
Tool/software:
During FW upgrade of binary generated from hex sci command in Linux from c2000 serial utility(customized as per our need), it is giving VERIFY ERROR. Although it is giving successful message in Flash Erase and after the load Program also. When checked in UniFlash Memory View the memory address 0x80000 (which is starting address) shows value as FF.
Earlier the binary was getting generated from CCS 12.0.0.00009 and c2000 toolchain version was 4_02_00. Now the CCS version is upgraded to 12.5.0 and c2000 toolchain is upgraded to 4_05_00 and binary is generated in Linux environment. The size of the binary has increased from 187KB to 191KB.
What can be the issue as memory map looks ok?