Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F29H85X-SOM-EVM: DACB output using EVM

Part Number: F29H85X-SOM-EVM
Other Parts Discussed in Thread: SYSCONFIG

Tool/software:

I’ve been working on getting the DAC to plot the reference voltage using the C2000. I’m a little confused on the F29 EVM pinout on enabling this:

 

Sysconfig

F29 Pin

SOM Board Output

HSEC DOCK Connector

DACA (A0/C24/DACA_OUT)

AIO160

This is also connected to ADCA Channel 0 so cant be used for DAC

 

DACB (E0/A24/DACB_OUT)

AIO202 (P3)

MCU_ADCIN_E0

Connector Pin J1B.95

Connector Pin J1B.95 is not connected to anything on the HSEC-180 Adapter Board

 

Am I missing some internal pinmux setting of the F29 chip that allows a different pin to be connected to the DAC output?