Part Number: F29H85X-SOM-EVM
Other Parts Discussed in Thread: HSEC180ADAPEVM, SYSCONFIG
Tool/software:
Hello Experts,
I am porting my old project from C28 to C29, and currently I am trying to use MCAN which is the same module, as per Migration Guide.
I would like to inquire about...
1. Could you please advise me as to which IOs and MCAN module are available on the EVM and thus the HSEC180ADAPEVM board? I am somewhat confiused. According to the pinout, the connections are labelled MCANA, MCAND and MCANE. I am unable to send or receive anything from the MCAN modules, as demonstrated by the example. It is possible that I am not approaching this correctly.
Kindly find attached the example files, I have updated example 4, rest is mostly same, just configured with MCANE.
MCAN.zip