Other Parts Discussed in Thread: C2000WARE
Tool/software:
Dear,
both C2000Ware_5_05_00_00 and C2000Ware_6_00_00_00 were installed.

but only C2000Ware_5_05_00_00 was shown on CCS 20.2.0



I need C2000Ware_6_00_00_00 package.
help me.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Dear,
both C2000Ware_5_05_00_00 and C2000Ware_6_00_00_00 were installed.

but only C2000Ware_5_05_00_00 was shown on CCS 20.2.0



I need C2000Ware_6_00_00_00 package.
help me.
Hi Insan,
I have looped in the CCS expert, and they should have a response back to you shortly.
Best Regards,
Delaney
Hi Insan,
Are you using CCS20.2 desktop?
Can you go to File -> Preferences -> Code Composer Studio Settings...

Then Under General -> Products , click on the refresh.

See if this helps reload your C2000ware version?
Please note that Resource Explorer (and the associated new project wizard) can lag what is available with ti.com. I confirmed that the C2000 team has not completed their handoff for C2000Ware v6 yet. To use v6 examples, you will have to do a manual import for now:
Thanks
ki
then CCS is dead.
Can you clarify what this means? Did CCS crash? Or hang?
Also, can you confirm that C2000Ware 6.0 is discovered by CCS?
https://www.ti.com/video/6369988068112
Thanks
ki
Yes, C2000Ware 6.0 is discovered by CCS.
I was able to reproduce the issue. I filed a ticket for this. Tracking link: https://sir.ext.ti.com/jira/browse/EXT_EP-12822
I noticed that the hang occurs when changing the device after the file is opened. If I change the device when first prompted when opening the *.syscfig file, it appears file: