This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28027: FLASH

Part Number: TMS320F28027

Tool/software:

   Hello, I added a bit too much code when using the 027 chip, and RAMM0_S1 reported an error. I can fix it
RAMM0_S1: Origin=0x000000, length=0x000600 Change to
RAMM0_S1: Origin=0x000000, length=0x000660. I found that the motor can run normally. Is there any risk? Or are there any other options,

   such as changing rom_comcessed_data:>RAMM0nM1 to rom_comcessed_data:>P_RAML0? It seems that the motor runs smoothly, which solution is better