Part Number: TMS320F28386D
Tool/software:
Hi,
is there a possibility to synchronize the 2 CLAs? Customer has to run same code/instruction clock synchrony. May be through a CPU instruction or CLB or external signal?
Regards, Holger
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28386D
Tool/software:
Hi,
is there a possibility to synchronize the 2 CLAs? Customer has to run same code/instruction clock synchrony. May be through a CPU instruction or CLB or external signal?
Regards, Holger
Hi Holger,
There is no CLA1-to-CLA2 MSGRAM available, so here are some other options:
Additionally, make sure that the lines of code after this takes the same amount of clock cycles if you want them to occur at the same time. If using identical code on both cores, make sure both projects have the same optimization level configured.
Best Regards,
Delaney