This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: FuSa SRAM10 example

Part Number: TMS320F28377D

Tool/software:

Hi,
the Safety Manual requires measures that are not supported by the SafeTI Diagnostic Library which will then be down to the user.
For example, SRAM10:
• There is no test routine in the SafeTI Diagnostic Library
• The Safety Manual requires the SRAM wrapper logic to be tested (Chapter 6.5.16 in the Safety Manual). Customer hasn't found a way to test arbitration. Is there an example of this?

The Excel sheet does not help either. Only actions of the user can be entered there. Here they would have liked only the used peripherals to be selected and the used functions from the SafeTI Diagnostic Library. The tool then calculates the residual error probabilities independently. 

Regards, Holger

  • Hi Holger,

    We don't currently have a test for RAM arbitration. I've reached out to our design team for more details. They may have an internal test case that could be adapted to something that could be shared in the SDL. Will update you when I hear back.

    Whitney

  • Hi Holger,

    I've discussed with the team and can provide some suggestion. You can test arbitration by triggering repeated accesses to the same memory block from two different controllers (CPU, CLA, DMA) at the same time. You can also mix up the types of accesses by executing code from the same memory block.

    For example, here's some pseudocode below showing the CPU executing code from LS0 while reading and writing to LS0 while the CLA also reads and writes to LS0.

    lsramArbitrationTest()
    {
        - Configure MemCfgRegs to assign MSEL and CLAPGM settings
        - Configure CLA tasks
        
        - Force CLA task so it starts executing claRWFromLS0();
        - Call cpuExecuteFromLS0()
        
        - Repeat these steps for all required LS RAMs
    }
    
    #pragma CODE_SECTION(cpuExecuteFromLS0, ".ls0ExecuteSec")
    void cpuExecuteFromLS0(void)
    {
    	DataInitValue = 0x12345678;
    	DataCheckValue = 0x12345678;
    
        // I'm hard-coding addresses here, but of course you can declare an array
        // and put it in LS0 if the RAM contains other things that you don't want
        // to overwrite at this point    
        DataWriteAddr = (uint32_t *)(LS0_START_ADDR + 0x450);
        DataCheckAddr = (uint32_t *)(LS0_START_ADDR + 0x450);
    
        // While this function executes from LS0, repeatedly write to LS0.
        // A CLA task will also be writing and reading to LS0 at the same time.
        for (i = 0; i < 200; i ++) {
            DataInitValue = DataInitValue + 0x12345678;
            *(DataWriteAddr++) = DataInitValue;
        }	
    
        // Read back the data that was written and make sure the writes were all
        // successful.
        for (i = 0; i < 200; i ++) {
            DataCheckValue = DataCheckValue + 0x12345678;
            if(*(DataCheckAddr++) != DataCheckValue)
            {
                ErrCount++;
            }
        }
    }
    
    // This function won't be able to be executed from LS0 since the RAM would 
    // need to be set to configured as CLA program RAM to execute
    #pragma CODE_SECTION(Cla1Task1, "Cla1Prog1")
    __interrupt void Cla1Task1(void)
    {
    	ClaDataInitValue = 0x456789AB;
    	ClaDataCheckValue = 0x456789AB;
    
        // I'm hard-coding addresses here, but of course you can declare an array
        // and put it in LS0 if the RAM contains other things that you don't want
        // to overwrite at this point    
        ClaDataWriteAddr = (long int *)(LS0_START_ADDR + 0x650);
        ClaDataCheckAddr = (long int *)(LS0_START_ADDR + 0x650);
    
        // Write and read back a bunch of data from LS0 while the CPU does the
        // same. Check that the accesses were successful.
        for (i = 0; i < 200; i ++) {
            ClaDataInitValue = ClaDataInitValue + 0x12345678;
            *(ClaDataWriteAddr++) = ClaDataInitValue;
    
            ClaDataCheckValue = ClaDataCheckValue + 0x12345678;
            if(*(ClaDataCheckAddr++) != ClaDataCheckValue)
            {
                ClaErrCount++;
            }
        }
    }

    You can also do a similar test between CPUs in the GS RAMs, synchronizing the start of the accesses using an IPC flag. You also need to make sure interrupts are disabled while performing these checks.

    Whitney

  • Hi Whitney,
    thanks for the answer. 

    Customer is not sure about the SRAM10 requirement. What does this test (Chapter 6.5.16 in the Safety Manual) exactly mean:

    "A Software Test of SRAM wrapper logic should provide diagnostic coverage for arbitration between different Masters having access to the particular SRAM and correct functioning of access protection. This is in addition To the test used to provide coverage of SRAM bit cells (See Section 6.3.12)."

    What does the context mean with

    • SRAM wrapper logic
    • diagnostic coverage
    • arbitration between various masters
    • access to the particular SRAM
    • access protection

    Should the test test test the hardware of the TMS320 or the implementation of the software by the user? 

    Regards, Holger

  • This is a test of the RAM hardware. SRAM wrapper logic includes things like arbitration, access protection, and the ECC/parity checker. The SDL already provides some code for performing a test of the ECC/parity checker logic. I don't think we have an access protection test in the F2837x SDL, but we do have an example for F2838x that should be similar.

    As for the part about the bit cells, the RAM of course has ECC/parity protection. If required, the SDL also provides a March test to proactively write and read back patterns in RAM.

    Whitney