Part Number: F29H85X-SOM-EVM
Tool/software:
Hi Champ,
I am reconfirming for my customer.
My customer wants to receive data with multiple Rx buffers instead of Rx FIFIOs, but doesn't know how to configure sysfg.
I have already read the "34.5.16.2 Rx Buffer and FIFO Element" section of F29x's TRM. According to TRM, up to 64 Rx buffers and two Rx FIFOs can be configured in the Message RAM.
The following screenshot shows the configuration page for RX MSG RAM. It does not appear to be able to configure the number of Rx buffers (but the number of Tx buffers can be configured).

And here are two other questions:
- Is there a feature difference between FIFO0 and FIFO1?
- How can I quickly determine the real start address of the Rx FIFO0 configured above?
Look forward to your response.
Thanks and regards,
Zeyan Li