Tool/software:
Hi Team,
I'm currently working on C2000 motor control SDK.
Trying to run the pump, here I'm facing an issue when I try to run the pump my debugger keeps disconnecting all of a sudden.
I have entered all my motor control parameters and as well as hardware parameters in user_mtr1.h file.
I have mentioned the motor parameters below:
Voltage - 24V
Current :10A
1.Rs - 0.1173
2.Ld - 0.000328
3.Lq - 0.00057
4.Flux_VpHz - 0.0626
5.INERTIA_Kgm2 - 0.0000268