Tool/software:
Hello, experts.
when the boot project jump to APP,how should the TMS320F28377D clear the memory which boot used?
Did I need to clear the “.ebss”, “.stack”, or “.TI.ramfunc” sections which boot used?
Look forward to your reply.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello, experts.
when the boot project jump to APP,how should the TMS320F28377D clear the memory which boot used?
Did I need to clear the “.ebss”, “.stack”, or “.TI.ramfunc” sections which boot used?
Look forward to your reply.
Hello,
In general, yes, but it depends. There could be conflicts when you switch from the bootloader to the app if you didn't take adequate care in the linker command files to separate them and avoid conflicts/overlaps. However, when you switch from the bootloader to the app, if you go through the C initialization routine (provided by the compiler), it will initialize whatever the application needs in RAM and initialize the SP before arriving at main(). In the process, it may end up overwriting some RAM areas that were being used earlier by the bootloader. This should not be an issue since you are not going to switch back live to the bootloader from the application.
Please refer to this thread: TMS320F280049C: Will there be a memory conflict when the bootloader and the app share a RAM area?
Best,
Matt