Part Number: TMS320F28379D
Tool/software:
Hi Team,
We are facing an issue with the C28xx_CPU1 after flashing the code. Within one minute of flashing, we get the following errors.
C28xx_CPU1: Error: (Error -1044 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 12.7.0.00105)
C28xx_CPU1: Trouble Halting Target CPU: (Error -1135 @ 0x8163B) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 12.7.0.00105)
C28xx_CPU1: Unable to determine target status after 20 attempts
C28xx_CPU1: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging.
This issue consistently occurs within one minute of flashing the code. We have verified the hardware connections and the debug probe configuration, and have also tried resetting the probe as suggested, but the issue persists.
Could you please assist us in identifying the root cause and suggest any potential fixes or workarounds? If any additional logs or diagnostic data are needed, we will be happy to provide them.
Looking forward to your guidance.