Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Hi I am now integrating the HWBIST micro run with CPU1 of our system, I use the Diagnostic library with the version C2000Ware_5_02_00_00.
In the beginning, the system is working(at least the working count in TimerISR looks good), but after the SCI FIFO RX INT is triggered, then the system looks crashed during the HWBIST micro run. The figure below is when the system crash.
And I have checked all the LSRAM of CPU1, the memory from RAMLS0 to RAMLS5 and RAMLS7 looks corrupted like the figure below (RAMLS6 is used for CLA program), they are all the data with same pattern(
0000 0000 0000 0000 0000 0000 0000 0000 081B 0000 0000 001F E946 003F 0001 0001)

Do you have any idea or hint of this?