This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: F28377D Run Issue

Part Number: TMS320F28377D

Tool/software:

Dear Expert:

When the 28377D dual-core is running, if the code on CPU1 runs abnormally and triggers a watchdog reset, CPU2 will also reset. However, at this time, it is prone to program boot failure and freezing. After the simulator runs online and detects an anomaly in CPU1, CPU2 will also reset. Once CPU2 fails to run, After CPU1 runs abnormally again and triggers a reset, it will get stuck in the initialization function "IPCBootCPU2(C1C2 ROM BOOTMODE BOOT FROM FLASH)". Eventually, neither CPU1 nor CPU2 can boot successfully.