Part Number: TMS320F2809
Other Parts Discussed in Thread: SYSBIOS
Tool/software:
Hi everyone
I have a question regarding the SYS/BIOS timer functionality, and I’m not sure if it works as expected. I’ve found multiple documents and forum posts that all seem to say different things.
What I expect is that when I call Timer_start(), it should reset the counter of the timer and also clear all interrupt flags. If the timer was already running before, it should not stop, but simply reset. Calling Timer_stop() should stop the timer.
However, I’ve found multiple forum posts saying that Timer_start() does not reset the timer and that this behavior doesn’t work. Some documentation mentions that there was a bug in the timer module, while other sources say it never reset the timer in the first place. Then, yet another SYS/BIOS document claims that it does reset the timer.
So, what I’d like to know is:
- What exactly do
Timer_start()andTimer_stop()do? - What happens if I call
Timer_start()when the timer is already running? Is that a problem? Do I have to callTimer_stop()first? - Which function call actually resets the timer, and which one clears the interrupt flags?
- Was there indeed a bug in an earlier version of SYS/BIOS, and if so, in which version was it fixed?
- Which is the correct documentation for SYS/BIOS version 6.83.0.18?
It would be great to get more details on this, because we have a system that isn’t 100% reliable, and we’re not sure whether the issue is with the timer module itself or the way we’re using it or something completely different.
Thank you very much.
Kind regards,
Dominik