This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] F29x Processor: Frequently Asked Questions

Part Number: F29H859TU-Q1

Tool/software:

Where can I find answers to frequently asked questions related to using the F29x processor?

  • For reference, please see F29x General FAQ for other IP/peripherals

    F29x Processor Frequently Asked Questions

    What is the difference between F28x and F29x for internal DCDC control?

    • F29x does not have an internal DCDC.

    Is there a plan to distribute the C29 instruction set?

    • There is no plan to provide C29 instruction set. We are planning to add list of intrinsic's with their description provided by C29 compiler.

    In linker command file, I changed the CPU entry point (CORE0_APP_START) and flashed the device with generated out file. Now I cannot re-flash the device with new program. How can I fix this error?

    • User should not change the codestart address for CPU1, this needs to be at 0x10001000. In case you have made the mistake and not able to re-flash the device, change the device boot mode from Flash Boot to Wait Boot, do a device reset or power cycle and connect back and re-flash the valid code.