Part Number: F29H859TU-Q1
Tool/software:
Where can I find answers to frequently asked questions related to System Control on F29x devices?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: F29H859TU-Q1
Tool/software:
Where can I find answers to frequently asked questions related to System Control on F29x devices?
For reference, please see F29x General FAQ for other IP/peripherals
F29x System Control Frequently Asked Questions
When CPU1 is running, can CPU3 be in a low-power mode, such as standby? When CPU3 is running, can CPU1 be in standby mode? Does the F29 support this scenario where one CPU is in low-power mode and the other CPU is running at full speed? Additionally, would the reduction in power consumption be significant in this case?
If CPU1 is in a fault state, can CPU3 continue to operate normally? Conversely, if CPU3 is in fault state, can CPU1 continue to operate normally?
On F28x, spread spectrum input to the PLL is not supported. Has this changed for F29x, or is the PLL identical to F28x?