This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dsp28335



Hello! happy new year.

          I want to you give me some way to solve the poblem that when I program flash of the dsp28335, the ccs3.3 displays "The device is in limp mode,.....".But in the same time, some of the target boards is , some of the targegt boards is not. they are same. Is some of the dsp28335 bad?  or another poblem?

        thank You again!

                                                                      Zhiping Yu

  • zhinping Yu said:

    Hello! happy new year.

              I want to you give me some way to solve the poblem that when I program flash of the dsp28335, the ccs3.3 displays "The device is in limp mode,.....".But in the same time, some of the target boards is , some of the targegt boards is not. they are same. Is some of the dsp28335 bad?  or another poblem?

            thank You again!

                                                                          Zhiping Yu

    It sounds like the input clock is not properly connected to the device.

    Please check the input clock to the DSP. Also, check XCLKOUT pin to ensure device is not in limp mode. SYSCLKOUT frequency in limp mode could be from 1 - 5 MHz.

    Regards

    Lori

  • There was a bug... I posted this picture and my question, and only the picture is sent...

    Actually, I have a problem with Piccolo F28027. I tried to adjust crystal oscilator and the processor has gone in limp mode...

    CCS 3.3 displayed message from the picture attached in my previous post... So, this message is present whenever I try to flash a program on processor F28027...

    I tried to flash a program on another F28027 and It works OK...

    Do you know how to solve this problem?

    Regards

    Nikola.