Tool/software:
Hi All,
X-bar INPUT1~3 are connected to the TZ of the ePWM module.
I cannot tell from the TRM whether INPUT4-6 can be used as a trip zone via ePWM X-BAR.
Please let me know if there is a register setting method or sample code.
According to Figure 9-1, INPUT1 to 6 can be connected to the ePWM X-bar, but can INPUT 7 to 12 also be connected to the ePWM X-bar?
Best Regards,
Ito