Other Parts Discussed in Thread: C2000WARE, SYSCONFIG, UNIFLASH
Tool/software:
Hello,
I am unable to flash my program to CPU2 in F28P65x using CCS Theia 20.2. I am trying to run the example from C2000Ware_6_00_00_00\driverlib\f28p65x\examples\c28x_dual\empty_projects where in I have two CCS projects - one that needs to be flashed to CPU1 and one that needs to be flashed to CPU2. I want to use Flash Bank 0, Bank 1 and Bnak 2 in order to flash from CPU1 and Flash Bank 3 and Flash Bank 4 to flash from CPU2. I am able to succesfully build both the projects. When I try the "Flash Project" option in CCS Theia to flash CPU1, it works. However, when I do the same for CPU2 I get the following error. Please help.