Part Number: LAUNCHXL-F28P55X
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Hi
Where can I find the explanation and implementation of these two modules in the documents or in the dual_axis_servo_drive code?

Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LAUNCHXL-F28P55X
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Hi
Where can I find the explanation and implementation of these two modules in the documents or in the dual_axis_servo_drive code?

Thanks
Luca,
I have assign this to our motor code expert. He will reply soon on your question. We appreciate your patience.
Regards,
Sumit
Hi,
I don't see documentation that explains it further, only other thing is https://www.ti.com/lit/ug/spruip4/spruip4.pdf?ts=1756308970299
Here is the related code for SVGEN and PWM comparator value setting. Hope it clarifies it.
//
// MACRO to :-
// 1. do SVGEN
// 2. do PWMupdates
//
FCL_SVGEN_PWM_PDATE_MACRO();
// FCL MACRO implementing SVGEN and PWM updates
// used in both PI CONTROL and COMPLEX CONTROL
//
#define FCL_SVGEN_PWM_PDATE_MACRO() \
/* \
* ----------------------------------------------------------------------------\
* Call the space vector gen. macro \
* ----------------------------------------------------------------------------\
*/ \
svgen2.Tb = (svgen2.Ubeta - svgen2.Ualpha) / 2; \
svgen2.Tc = svgen2.Tb - svgen2.Ubeta; \
\
svgen2.tmp2 = __fmax(__fmax(svgen2.Ualpha, \
svgen2.Tc), svgen2.Tb); \
svgen2.tmp2 += __fmin(__fmin(svgen2.Ualpha, \
svgen2.Tc), svgen2.Tb); \
\
svgen2.tmp1 = ((-svgen2.tmp2) / 2) + \
pMotor->FCL_params.carrierMid; \
\
/* \
* -----------------------------------------------------------------------------\
* Computed Duty and Write to CMPA register \
* -----------------------------------------------------------------------------\
*/ \
FCL_PWM_UPDATE_STYLE_3();
#define FCL_PWM_UPDATE_STYLE_3() \
*(pMotor->pwmCompA) = (uint32_t)(svgen2.Tc + svgen2.tmp1); \
*(pMotor->pwmCompB) = (uint32_t)(svgen2.Ualpha + svgen2.tmp1); \
*(pMotor->pwmCompC) = (uint32_t)(svgen2.Tb + svgen2.tmp1);
Best,
Kevin
Thank you.
But is the code you sent me that of SVGEN or that of PWM MACRO/PWM HV ?
Hi,
It is both. For PWM Macro see FCL_PWM_UPDATE_STYLE_3() function which calculates and sets the PWM compare values based on the SVGEN inputs. And pwmCompA/B/C pointer was already defined in FCL_initPWM() function earlier, so it writes directly to the EPWM CMPA register.
ptrMotor->pwmCompA = (uint32_t *)(basePhaseU + EPWM_O_CMPA);
ptrMotor->pwmCompB = (uint32_t *)(basePhaseV + EPWM_O_CMPA);
ptrMotor->pwmCompC = (uint32_t *)(basePhaseW + EPWM_O_CMPA);
Best,
Kevin
I ask one more thing.
The explanation of all modules used in dual_axis_servo_drive can be found by downloading designdrive?
Because I currently do not have it installed, although the code works since CCS is sufficient
Hi,
You can import into CCS and reference the below project directory that's in the https://www.ti.com/tool/C2000WARE-MOTORCONTROL-SDK installation.
C:\ti\c2000\C2000Ware_MotorControl_SDK_5_04_00_00\solutions\boostxl_3phganinv\f28p55x
Best,
Kevin