Part Number: TMS320F28386D
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi there,
I'm having an issue involving the eCAP peripheral. I'm using eCAP3 to capture the signal frequency from GPIO23, but the CTR register is overflowing and never transferring the value to the CAP1 register.
I’ve already checked the INPUTSEL setting — it’s set to 118 (I'm using SysConfig), and the module is in continuous mode.
I also tried changing the INPUTSEL to route a signal from the XBAR, and with that change, the peripheral works fine.
I also checked GpioDataRegs.GPADAT.GPIO23, and the register toggles normally between 0 and 1 as expected, but CAP1 still doesn’t update.
To reserve GPIO23, I configured it as a synchronous floating input.
Am I missing something? Are there any specific configurations I need to apply to GPIO23 before using it with eCAP?
Thank you for your guidance!