Part Number: LAUNCHXL-F280049C
Other Parts Discussed in Thread: C2000WARE, SFRA, TIDM-02007
Tool/software:
Hello,
I am working with the LAUNCHXL-F280049C and installed the C2000Ware MotorControl SDK v5.04.00.00.
According to the documentation, the TIDM-02007 Dual-Axis Motor Drive using FCL & SFRA on a single MCU should be included in the SDK under Solutions.
However, in my installation I cannot find the tidm_02007_dual_axis_motor_drive project (neither in the local SDK folder nor in the Resource Explorer inside CCS, which only shows Development Kits, Documentation, Libraries, and Resources – but no Solutions).
Could you please clarify:
-
Is TIDM-02007 still part of the MotorControl SDK, and if so, in which version?
-
Where can I download the CCS project files for F28004x (F280049C) Dual-Axis motor control?
-
Should I import it via Resource Explorer (Online), or is there a direct ZIP package available on the TI website?
Thank you very much for your support.