This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28379D: LAUNCHXL-F28379D

Part Number: LAUNCHXL-F28379D

Tool/software:

Hello

    could you please tell me that after I use the host computer to burn a program into the development board, how can I ensure that the development board still runs the burned program normally after being disconnected from the host computer?

  • Hi Mingshuo,

    You will want to make sure that you load the device with a flash-based project from the host program. If you use a flash program, you will see that the flash banks will be overwritten when CCS loads into the debug menu. This should mean that the program is burned onto the board, just make sure the boot switch is configured to boot from FLASH (check the LaunchPad user guide for this info).

    Regards,

    Peter