This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P650DK: Inquiry Regarding Power Supply Options for TMS320F28P650DK9.

Part Number: TMS320F28P650DK


Tool/software:

Dear TI Support Team,

I am writing to inquire about the power supply options for the TMS320F28P650DK9 microcontroller.

As I understand, this device includes an internal 1.2V regulator, which allows operation by supplying only an external 3.3V VDDIO and grounding the VREGENZ pin. This is a very useful feature for reducing PCB footprint.

However, according to the device’s datasheet, it appears that the overall power consumption is higher when using the internal 1.2V regulator compared to supplying an external 1.2V source. Consequently, I would expect the overall heat dissipation of the device to be higher when relying on the internal regulator.

With this in mind, I would like to ask the following questions:

1. Can the device reliably operate across the full datasheet-specified free-air temperature range (-40°C to +125°C) when only the external 3.3V VDDIO is provided and the internal 1.2V regulator is enabled?

2. Since enabling the internal 1.2V regulator seems to increase total power consumption and heat dissipation, this could be a disadvantage in high-temperature environments (e.g., above 100°C). Are there any documented specifications or application notes that detail the power/thermal dissipation characteristics of the device under both configurations (using the internal regulator vs. an external supply)?

3. What is TI’s recommended power supply design approach for this device (using the internal regulator vs. an external 1.2V supply)?

Thank you very much for your assistance.

Best regards,
Sangil Nam

  • Hello Sangil,

    Thanks for reaching out here. Appologies for the delayed response as I typed this up and it never sent.

    1) Yes, this is applicable for both internal VREG enabled and disabled.

    2) While using the internal regulator will increase power and temperature on the device, you also have to realize that by adding an external regulator/supply, you are adding an additional component with it's own heat and power dissapation. This does not necesssarily mean that you will save power/temperature by moving this external to the device.

    3) TI has the below app notes 

    https://www.ti.com/lit/an/spradg6/spradg6.pdf - Power Supply and Monitoring Solution for C2000 MCU Automotive Applications

    https://www.ti.com/lit/ds/sbvs144c/sbvs144c.pdf - Integrated MCU Power Solution for C2000Tm Microcontrollers

    The necessity of internal vs external regulator/supply is an application/system level careabout. If the goal is to reduce BOM/Area then the internal regulator is recommended. If optimal power/heat/performance is the goal, then an external source may be recommended.

    Best Regards,

    Zackary Fleenor

  • I sincerely appreciate your kind response.