Other Parts Discussed in Thread: C2000WARE
Tool/software:
Using Application Note SPRACM3E "Using the Fast Serial Interface (FSI) With Multiple Devices in an Application" as a starting point, Section 7.2.4 1 Lead and 8 Node F28002x Device Daisy-Chain Tests.
For an 8-node daisy-chain of F280039C (or ..25C, 49C) MCUs, is there any path forward on being able to reprogram/reflash the daisy-chain controllers over the Fast-Serial-Interface (FSI)? A separate physical layer communication network just to reprogram the controllers is not feasible.
The application is calling for being able to reprogram the nodes on the daisy-chain without individually connecting to each one, programming one at a time. Instead being able to program them over the existing control communication network, in this case FSI.
I see there are use cases for reflashing over CAN and a few others in Ch 4 of the F280039C Technical Reference Manual, but nothing on FSI.