Part Number: TMS320F28388D
Tool/software:
Hi,
When I integrating the HWBIST in our system, we use the Micro-Run.
When I am doing the CPU2 HWBIST, it will get the 0x19 retrun value of the STL_HWBIST_runMicro(), which means the HWBIST detected a logic error. I changed another chip, it face the same problem.
But when I did the HWBIST on CPU1, it can successfully finish the HWBIST 99% coverage with no error.
So I have some questions below:
1. Is there any difference of the HWBIST initial between the CPU1 or CPU2?
2. What can I do if this logic error happened?
The library version:
TI Release: C2000 Diagnostic Library v5_02_00_00