Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28023: interrupt on aio10

Part Number: TMS320F28023
Other Parts Discussed in Thread: C2000WARE

Tool/software:

Hi TI Experts,

I am working on tms320f28023 
i need to configure intrrupt on AIO10 to use it for uart receive through bit banking method,

Any guidance, documentation links, or example projects would be greatly appreciated.

Thanks in advance!

  • Hello,

    Please allow another day for me to formulate my response. Thanks for your patience. 

    Best Regards,

    Allison

  • Ranjith,

    While we do not have dedicated examples for bit banging, we do have several examples to reference in terms of general GPIO configuration and CPU timers within the C2000Ware device support directory for F2802x (C:\ti\c2000\C2000Ware_6_00_00_00\device_support\f2802x\examples\drivers). I'd recommend looking into these and perhaps using a CPU Timer that matches your baud rate. On the receive, you can also leverage external interrupts on this device which can be selected negative or positive edge-triggered triggered. Here are some examples to reference:

    • cpu_timer example
    • external_interrupt example
    • gpio_setup example
    • timed_led_blink example
    Feel free to create another thread with more specific peripheral configuration questions when trying to implement this. 

    Best Regards,

    Allison