Other Parts Discussed in Thread: CONTROLSUITE
Hello,
I've installed and updated CCSv4 and controlSuite on two computers, one running Win XP (SP 2) and one with Win 7. When I plug two USB cables (J2 and J20 on the card) into the Win 7 machine, XDS100 appears in device manager (as explained in http://processors.wiki.ti.com/index.php/XDS100#Installation_for_Code_Composer_Studio_v4.x) and I can normally connect to both 28x and M3 targets.
The problem is that when I connect USB cables to the computer with Win XP an USB tray icon appears shortly but nothing new appears in device manager. When I try to connect to 28x or M3 target I get an error message:
Error connecting to the target:
(Error -151 @ 0x0)
This utility failed to open the adapter for a custom emulator.
The adapter returned an error.
(Release 5.0.429.0)
I tried reinstalling CCSv4 two times but it didn't help. What could be the problem?
Regards, Josip