Tool/software:
I am working on the protection for TMS320F28379D that is used in a few commercial products. Some questions about PIN's internal protection circuitries:
1) Do all of pins have the internal protection circuitries for OCP, OVP, ESD and so on?
2) What are the specific internal protection circuitries? In other words, how do these circuitries look like?
3) Is it necessary to add the external protection circuitries for some pins? If yes, what pins are they and what kind of protection circuitries are needed/recommended?
Thanks