Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2808: ADC_Calibration assembly file

Part Number: TMS320F2808

Tool/software:

Hey Support Team,

I was searching for the ADC_calibration for TMS320F2808 MCU, But i see that this section has been removed from the datasheet. 
I searched more in another devices like TMS320F2833x and i found there is calibration for the ADC.

in Brief, the ADC_cal() is called before ADC_ClkEnable and there is a assembly file is called >> DSP2833x_ADC_cal.asm

it contains:

.def _ADC_cal
.asg "0x711C", ADCREFSEL_LOC

;-----------------------------------------------
; _ADC_cal
;-----------------------------------------------
;-----------------------------------------------
; This is the ADC cal routine.This routine is programmed into
; reserved memory by the factory. 0xAAAA and 0xBBBB are place-
; holders for calibration data.
;The actual values programmed by TI are device specific.
;
; This function assumes that the clocks have been
; enabled to the ADC module.
;-----------------------------------------------

.sect ".adc_cal"

_ADC_cal
MOVW DP, #ADCREFSEL_LOC >> 6
MOV @28, #0xAAAA ; actual value may not be 0xAAAA
MOV @29, #0xBBBB ; actual value may not be 0xBBBB
LRETR

-----------------------
I undestood that the addresses #0xAAAA and #0xBBBB are placeholders, we should change them with the ADC_Cal values that stored in OTP for the device.

The problem is that i cant find these addresses that stored inside it the ADC calibration values to replace them with the placeholders 0xAAAA,#0xBBBB.

---
My Questions are:

1- Is there any ADC_Calibration values are stored in the OTP address ?
2- If it is, How can i know the OTP Addresses that stores the ADC_CAlibration values?

Thanks, 
Abdelrahman