Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388S: Register Reserved Fields are Non-Zero

Part Number: TMS320F28388S

Tool/software:

Greetings,

I am working with the USB, and have noted that in at least two cases, registers are reporting non-zero values in reserved parts of registers.  For example, in the case of USBTXIS, the four least significant bits are defined.  The rest of the register is reserved.  But I am receiving a value of 0x6030.  In the other case, USBBEPIDX, again, the least significant four bits are defined.  But I am receiving a value of 0x78.  In both cases, the TRM states that the fields should read back as 0.  Is this an issue?

Thank you,

Ed