This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28P55X: Issue with importing launchpad examples

Part Number: LAUNCHXL-F28P55X
Other Parts Discussed in Thread: C2000WARE

Tool/software:

Hello,

I have installed the c2000ware 5.05 with the examples to use the launchpad f28P55x. I have installed CCS 12.2. I have come accross the problem that when I import a project, the ccs throws an error saying that I do not have the family libraries. However, I have installed the c2000 product family libraries. How can I solve this issue?

Regards,

David

  • Hello,

    I tested loading an example with this launchpad using the same version of CCS and C200Ware and did not see this error.
    I would recommend the following steps:
    1. Check if there are any missing updates within CCS via the Help > Check for Updates tab
    2. Re-run the CCS installer and make sure C2000 microcontrollers is selected, as per below:

    Regards,

    Susan