Part Number: TMS320F28027F-Q1
Tool/software:
Several defects are discovered on the Post controller project around of 3.3 units per week are being disposed as scrap by internal issues on the microcontroller U627 (17052086-01) The microcontroller is being used to drive a 3-phase fan and in an electrical charger control module. The issue is discovered during functional test specifically during the Fan tests. It has been taken three suspected units, and then we tried to connect the microcontroller (MCU) to our application software and through Blackhawk Debug Probe. The communication failed with the MCU with part number: 17052086-01. The three suspected units present the same communication failure.
The reported communication issue could not be verified on bench or ATE from Texas Instrument.