This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-DC-DC-BUCK: Buck parameters for Rev 2.1 design

Part Number: TIDM-DC-DC-BUCK
Other Parts Discussed in Thread: SYSCONFIG, BOOSTXL-BUCKCONV

Tool/software:

Hello

I am using the newer version of TIDM-DC-DC-BUCK (F280049C launch pad with Buck converter where C9 is depopulated). I read in some thread on this forum that C8 was changed to a different C value with a different ESR in the newer board. I want to make sure the values I have in CCS main.syscfg are correct. The following came with the default project -

Are these values updated or do I need to change anything? (Output C8 Elec Capacitance and it's ESR)

Thanks,
Kamakshi