Part Number: TMS320F28P650SH
Tool/software:
I recently updated to 20.3.0, and the graph visualization feature is no longer working the way it used to. Now, instead of plotting a section of memory, the x-axis makes no sense whatsoever. It keeps increasing (to infinity?) and does not match the memory it is plotting. What I'd like to do is plot a section of memory, the way the graph used to do. This was incredibly useful when debugging algorithms storing signals, especially in circular buffers. Now, the 'Time' graph is virtually useless. This was one of my most valuable analysis tools, particularly the way it could plot several signal buffers simultaneously on the same axes. I'm devastated it's gone. Can we bring it back please? Or is there somewhere else I can access this tool now?
Thanks