Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D-EP: Question: Power supply sequence

Part Number: TMS320F28377D-EP

Tool/software:

I would like to konow bellows.

Please inform me.

1. Supply ramp rate

    About: supply ramp rate requirement in Datasheet 4.7.1 table 4-3

   Question: Is the requirement applied to only power-on state or power-on and power-off state? 

2.VDDIO and VDD

   About: Datasheet 4.7.1 discription: The voltage on VDDIO shold be greater than VDD or no less than 0.3V bellow VDD at all times.

   Question1: Is the requirement applied to power-off state?  ( in power-off state : /XRS is drived to low by external circuit. )

   Question2: If VDDIO is less than 0.3V bellow VDD, TMS320F28377D-EP's internal circuit iwill be dameged? 

   Background: Shottkey diode can`t use for high temeprature application, because of the diode's leakage current is too much at .high tempeature.  

  • 1. Supply ramp rate

        About: supply ramp rate requirement in Datasheet 4.7.1 table 4-3

       Question: Is the requirement applied to only power-on state or power-on and power-off state? 

    This is only for the power up state.  The only thing to avoid with power down, is:

    -VDD should not exceed VDDIO

    -Making sure there isn't an input to the device that will be >VDDIO as it ramps down.

    2.VDDIO and VDD

       About: Datasheet 4.7.1 discription: The voltage on VDDIO shold be greater than VDD or no less than 0.3V bellow VDD at all times.

       Question1: Is the requirement applied to power-off state?  ( in power-off state : /XRS is drived to low by external circuit. )

       Question2: If VDDIO is less than 0.3V bellow VDD, TMS320F28377D-EP's internal circuit iwill be dameged? 

       Background: Shottkey diode can`t use for high temeprature application, because of the diode's leakage current is too much at .high tempeature.

    Yes, I would want to ensure this compliance is met, even on power down.  The risk if VDD>VDDIO+0.3V is that we reverse bias some of the internal transistors and we get current sourced from VDD into VDDIO.

    Best,

    Matthew

  • Thank you.

    I understand.