Tool/software:
- When I look at the LAUNCHXL-F28P65X, I realize that BAW Oscillator which PN:LMK6CE02500CDLFT and CLOCK BUFFER are used for clocking in the schematic. Could I use 25 MHz oscillator instead of 25 MHz BAW Oscillator + CLK BUFFER for this application? What would TI suggest on this usage case?
- Also, In our design, the ETHERCAT will not be featuring, instead CAN-FD will be featured. For that purpose, I would like to know if CLOCK BUFFER is still needed in case EtherCAT is not featured, which means that single CLOCK is enough for MCU.?