This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: how to trigger multiple ADC conversion at regular interval

Part Number: TMS320F280049C

Tool/software:

i need to trigger ADC conversion at setting regular interval, these conversions may not be synchronous with ePWMs, sample frequency is much higher than ePWM, maybe 8 times

so i think i can use CPU timer to trigger ADC conversion, and i do not want that the CPU enter an interrupt service , i just need the timer to generate a regular time interval.

in the TRM the trigger setting description is not so clear, whether the CPU timer interrupt trigger the ADC conversion or the count down to zero event trigger the conversion. and DMA may be used to move the sample result to avoid interrupt CPU. 

  • Hi,

    Another EPWM signal (eg EPWM2) can be used in that case that can be Syncronized with the already configured EPWM(Eg EPWM1) instance.

    EPWM2 can run at the desired frequency required, this way the triggering can happen without intervening CPU. 

    BR,

    Nilesh