This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800132: EPWM Initialization issue

Part Number: TMS320F2800132
Other Parts Discussed in Thread: C2000WARE

Tool/software:

I am Trying to work with EPWM , using the following code but could not start . Whats missing ?

// Included Files
//
#include "f28x_project.h"
#include "f280013x_device.h"
//
// Main
//

unsigned int i = 0;
void init_ePWM3(void);
void init_epwm2(void);
void main(void)
{
    InitSysCtrl();

    EALLOW;
    GpioCtrlRegs.GPBGMUX1.bit.GPIO32    = 1;
    GpioCtrlRegs.GPBMUX1.bit.GPIO32     = 0;
    GpioCtrlRegs.GPBPUD.bit.GPIO32      = 0;
    GpioCtrlRegs.GPBDIR.bit.GPIO32      = 1;
    EDIS;
   
    //init_ePWM3();
    init_epwm2();
    while(1)
    {
       
        // GpioDataRegs.GPBSET.bit.GPIO32 =  1;

        // DELAY_US(1000000);

        // GpioDataRegs.GPBCLEAR.bit.GPIO32 =  1;

        // DELAY_US(1000000);
        // if(EPwm3Regs.TBCTR == 0)
        // {
        //     i++;
        // }

    }

}

/* ePWM 3 Configurations*/

void init_ePWM3(void)
{
    EALLOW;
        //
    // Enable EPWM3 clock
    //
    CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 0;

    CpuSysRegs.PCLKCR2.bit.EPWM3 = 1;

   
    GpioCtrlRegs.GPHMUX1.bit.GPIO227    = 3;

   
    GpioCtrlRegs.GPHMUX1.bit.GPIO230    = 3;

    //
    // Disable TBCLK before config
    //
   
    //
    // Step 1: Configure GPIO230 as EPWM3A and GPIO227 as EPWM3B
    //
    // GpioCtrlRegs.GPHGMUX1.bit.GPIO227 = 1;
    // GpioCtrlRegs.GPHGMUX1.bit.GPIO230 = 1;
    //GPIO_SetupPinMux(230, GPIO_MUX_CPU1, 1);   // MUX = 1 → EPWM3A
    //GPIO_SetupPinOptions(230, GPIO_OUTPUT, 0);


    GpioCtrlRegs.GPHPUD.bit.GPIO227   = 0;   // Enable internal pull-up (0=enabled, 1=disabled)
    GpioCtrlRegs.GPHQSEL1.bit.GPIO227 = 0;   // Qualification = sync to sysclk

    GpioCtrlRegs.GPHPUD.bit.GPIO230   = 0;   // Enable internal pull-up (0=enabled, 1=disabled)
    GpioCtrlRegs.GPHQSEL1.bit.GPIO230 = 0;   // Qualification = sync to sysclk


    //GPIO_SetupPinMux(227, GPIO_MUX_CPU1, 1);   // MUX = 1 → EPWM3B
    //GPIO_SetupPinOptions(227, GPIO_OUTPUT, 0);

    //
    // Step 2: Time-Base Setup
    //
    EPwm3Regs.TBPRD = 1250;               // Period register → sets freq
    EPwm3Regs.TBCTL.bit.CTRMODE = 2;      // Up-Down count mode
    EPwm3Regs.TBCTL.bit.PHSEN   = 0;      // Disable phase loading
    EPwm3Regs.TBCTL.bit.HSPCLKDIV = 1;    // Clock divide = /2
    EPwm3Regs.TBCTL.bit.CLKDIV    = 0;    // Clock divide = /1
   

    // Counter Compare Register
    EPwm3Regs.CMPCTL.bit.SHDWAMODE      = CC_SHADOW;
    EPwm3Regs.CMPCTL.bit.SHDWBMODE      = CC_SHADOW;
    EPwm3Regs.CMPCTL.bit.LOADAMODE      = CC_CTR_ZERO;
    EPwm3Regs.CMPCTL.bit.LOADAMODE      = CC_CTR_ZERO;

    //
    // Step 3: Compare Values (Duty Cycle)
    //
   
    EPwm3Regs.CMPA.bit.CMPA = 625;        // 50% duty for A
    EPwm3Regs.CMPB.bit.CMPB = 312;        // 25% duty for B

    //
    // Step 4: Action Qualifier
    //
    // For EPWM3A: set on ZERO, clear on CMPA up

    EPwm3Regs.AQCTLA.bit.CAU = 2;         // SET on Zero
    EPwm3Regs.AQCTLA.bit.CAD = 1;         // CLEAR on Compare A up

    // For EPWM3B: set on ZERO, clear on CMPB up
    EPwm3Regs.AQCTLB.bit.CBU = 1;         // SET on Zero
    EPwm3Regs.AQCTLB.bit.CBD = 2;         // CLEAR on Compare B up


    CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 1;
    //CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 1;   // Enable TBCLK Config
    EDIS;
}

void init_epwm2(void)
{
    EPwm3Regs.TBCTL.bit.CLKDIV = 0;
    EPwm3Regs.TBCTL.bit.HSPCLKDIV = 1;
    EPwm3Regs.TBCTL.bit.CTRMODE = 2;
    EPwm3Regs.AQCTLA.all        = 0x0006 ;
    EPwm3Regs.TBPRD             = 37500;
}

But could not initiate the EPWM . GPIO Muxing is achieved . 

  • If anyone can guide me what are the steps to be taken care for register level programming

  • Rishabh,

    Have you tried ePWM examples in C2000ware to check which feature you want to use? Location is C2000Ware installation directory as follows: C:\ti\c2000\C2000Ware_5_05_00_00\driverlib\f280013x\examples\epwm

    This is first point for getting started and then you can go register level eventually.

    Regards,

    Sumit

  • Hi Sumit , Thanks for replying

    Yes i have tried it that and works fine . But code snippet represents Register mapped configuration from TRM understanding . 

    I tried some other configuration found it to be working  Please find the working code ,

    #include "f28x_project.h"
    #include "f280013x_device.h"

    #define STAND_ALONE_EPWM
    //
    // Main
    //
    unsigned int i = 0;

    void Gpio_ePwm(void);
    void ClockConfig(void);
    void init_ePWM3(void);
    void start_ePWM(void);

    void main(void)
    {
    InitSysCtrl();
    InitGpio();
    EALLOW;

    GpioCtrlRegs.GPBGMUX1.bit.GPIO32 = 1;
    GpioCtrlRegs.GPBMUX1.bit.GPIO32 = 0;
    GpioCtrlRegs.GPBPUD.bit.GPIO32 = 0;
    GpioCtrlRegs.GPBDIR.bit.GPIO32 = 1;


    EDIS;
    //
    // Initialize PIE and clear PIE registers. Disables CPU interrupts.
    //
    DINT;
    InitPieCtrl();
    IER = 0x0000;
    IFR = 0x0000;
    //
    // Initialize the PIE vector table with pointers to the shell Interrupt
    // Service Routines (ISR).
    //
    InitPieVectTable();

    //
    // Enable Global Interrupt (INTM) and realtime interrupt (DBGM)
    //
    EINT;
    ERTM;


    /* Step 1 : Assigns GPIO 227 Pin 20 DRIVEB --> EPWMB and GPIO 230 Pin 21 DRIVEA --> EPWM A*/
    Gpio_ePwm();
    /* Step 2 : Configure EPWM Clock, Disable TIME BASE CLOCK for Setting up the Registers*/
    ClockConfig();
    /* Step 3 : Configure Time- Base , Capture Compare , Action Qualifier Blocks*/
    init_ePWM3();
    /* Step 4 : Enable Time BASE CLOCk and start the ePWM Module*/
    start_ePWM();


    while(1)
    {
    // GpioDataRegs.GPASET.bit.GPIO12 = 1;
    GpioDataRegs.GPBSET.bit.GPIO32 = 1;
    DELAY_US(1000000);
    GpioDataRegs.GPBCLEAR.bit.GPIO32 = 1;
    DELAY_US(1000000);

    }

    }

    /*GPIO Muxing Channels*/
    void Gpio_ePwm(void)
    {
    EALLOW;
    /*GPIO Muxing*/
    GpioCtrlRegs.GPHMUX1.bit.GPIO227 = 3;
    GpioCtrlRegs.GPHMUX1.bit.GPIO230 = 3;

    GpioCtrlRegs.GPHDIR.bit.GPIO227 = 1; // output
    GpioCtrlRegs.GPHDIR.bit.GPIO230 = 1; // output

    GpioCtrlRegs.GPHPUD.bit.GPIO227 = 1; // Enable internal pull-up (0=enabled, 1=disabled)
    GpioCtrlRegs.GPHQSEL1.bit.GPIO227 = 0; // Qualification = sync to sysclk

    GpioCtrlRegs.GPHPUD.bit.GPIO230 = 1; // Enable internal pull-up (0=enabled, 1=disabled)
    GpioCtrlRegs.GPHQSEL1.bit.GPIO230 = 0; // Qualification = sync to sysclk
    EDIS;
    }

    /* ePWM Clock initialization*/
    void ClockConfig(void)
    {

    /*
    The TBCLKSYNC bit in the peripheral clock enable registers allows all users to globally synchronize all enabled
    ePWM modules to the time-base clock (TBCLK). When set, all enabled ePWM module clocks are started with
    the first rising edge of TBCLK aligned. For synchronized TBCLKs, the prescalers for each ePWM module must
    be set identically.
    The proper procedure for enabling ePWM clocks is as follows:
    1. Enable ePWM module clocks in the PCLKCRx register
    2. Set TBCLKSYNC= 0
    3. Configure ePWM modules
    4. Set TBCLKSYNC= 1
    */
    EALLOW;
    CpuSysRegs.PCLKCR2.bit.EPWM3 = 1; // Enable EPWM3 Clock
    CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 0; // Disable Time Base Clock
    EDIS;
    }

    void start_ePWM(void)
    {
    EALLOW;
    CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 1; // Disable Time Base Clock
    EDIS;
    }

    /* ePWM 3 Configurations for TB , AQ and CC block */

    void init_ePWM3(void)
    {
    // Time Base Block Congigurations
    EPwm3Regs.TBPRD = 1500 ; // Period register → sets freq
    EPwm3Regs.TBCTL.bit.CTRMODE = 2 ; // Up-Down count mode

    EPwm3Regs.TBCTL.bit.HSPCLKDIV = 1 ; // Clock divide = /2
    EPwm3Regs.TBCTL.bit.CLKDIV = 0 ; // Clock divide = /1

    #ifdef STAND_ALONE_EPWM
    EPwm3Regs.EPWMSYNCINSEL.bit.SEL = 0 ; // Disable Sychronizations
    EPwm3Regs.TBCTL.bit.PHSEN = 0 ; // Disable phase loading
    //EPwm3Regs.TBCTL.bit.SWFSYNC = 0 ; // Disabled Software Force Sync
    #endif

    // Counter Compare Block Configurations

    EPwm3Regs.CMPCTL.bit.SHDWAMODE = 0 ; // Double Buffer via CPU Shadow Register
    EPwm3Regs.CMPCTL.bit.SHDWBMODE = 0 ; // Double Buffer via CPU Shadow Register
    EPwm3Regs.CMPCTL.bit.LOADAMODE = 0 ; // Load to Active Register when CTR = 0
    EPwm3Regs.CMPCTL.bit.LOADBMODE = 0 ; // Load to Active Register when CTR = 0

    // Action Qualifiers Block Configurations

    EPwm3Regs.AQCTLA.bit.CAU = 2 ; // Set High EPWM 3A When CTR = CMPA while Up Count.
    EPwm3Regs.AQCTLA.bit.CAD = 1 ; // Clear EPWM 3A When CTR = CMPA while Down Count.
    //EPwm3Regs.AQCTLA.bit.PRD = 2 ;

    EPwm3Regs.AQCTLB.bit.CBU = 1 ; // Clear EPWM 3B When CTR = CMPB while Up Count.
    EPwm3Regs.AQCTLB.bit.CBD = 2 ; // Set High EPWM 3B When CTR = CMPB while Down Count.
    // EPwm3Regs.AQCTLA.bit.ZRO = 2 ;
    // Set the Compare Values (Duty Cycle)

    EPwm3Regs.CMPA.bit.CMPA = 1450 ; // 50% duty for A
    EPwm3Regs.CMPB.bit.CMPB = 50 ; // 25% duty for B

    }