Part Number: TMS320F28P550SJ
Other Parts Discussed in Thread: CCSTUDIO
Tool/software:
Hi champs,
I am asking this for our customers.
CCS 12.8.1
C2000 F28003x/P55x/P65x
The user has studied CCS commands in
https://software-dl.ti.com/ccs/esd/documents/ccs_projects-command-line.html
However, the user does not put project folders under the workspace folder. That is, the projects are in a total different folder/drive from the workspace folder.
In this case, how does the user handle <workspace_path>?
For example, there are two projects Project A and Project B in C:\ti\A and C:\ti\B.
But the workspace is in D:\workspace
Can all the CCS command lines work? Or how should the user do?
Besides, for CCS Theia 20.3+, is it still the same as CCS 12.8.1 in this case? If not, what should the user do?